Wi-Fi mode connection — Basic Hub

AP mode (Wi-Fi) is used to commission the Basic Hub via wireless (Wi-Fi) rather than Ethernet. There might be a situation when Ethernet mode of commissioning is not available for commissioning the Basic Hub. For example, the router location or commissioning new home with router not available yet, therefore, the installer can choose AP mode.
Pre-requisite:
  • The Wi-Fi mode is supported in the Basic Hub. To update the latest firmware, connect the hub to the Ethernet (see Ethernet mode connection- SmartHUB Wiser Hub Gateway ).

  • To commission the basic hub by AP mode, a user must have an account in the App. For more information on creating a user account see Creating an account.

  • The Wi-Fi in the mobile phone/tablet must be active.

  • The Wi-Fi router, basic hub, and mobile phone/tablet must be as close as possible.

  1. Login in to the App.
  2. (See A, B) Select the home where the Hub gateway is located (A) then tap the + icon (B) or Add Device.

  3. On the Add device page, tap Add manually (See C). Then select Basic HubWiser Gateway under the listed devices.
    NOTE: Do not tap Auto Scan as the Basic Hub is not visible in Wi-Fi mode under Auto Scan.
    NOTE: The list of the devices vary based on country.
    NOTE: The device images in below screenshot is only for representation purpose. However, the real screen in the app varies based on the devices available in your country.

  4. Upon selecting Basic Hub, you will receive option to select the modes of commissioning the Basic Hub. Select Connect with WiFi for commissioning (See D).

  5. Click Ready to Configure (See E) when you reach the Connect with WiFi page.

       
  6. An animation is displayed about How to pair device. Follow the steps to complete the pairing, tap Confirm Internet LED blinks (See F) and tap Start Configuration (See G). Then you will be prompted to a page showing the available Wi-Fi network. Enter the Wi-Fi password and tap Next .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?